2.1 Using the License Management Feature

The license management feature registers and manages newly acquired licenses for CS+ and related tools on the host machine by starting the License Manager window using the method below.

-

From the Windows the [Start] menu, select [Programs] >> [Renesas Electronics CS+] >> [License Manager]

Remark

In Windows 8 or Windows 8.1, click on [License Manager] on the start screen.

 

The following functionality will be restricted if a license is not registered.

-

Below are the maximum code sizes that can be developed.

-

RH850 family: 256 Kbytes

-

RX family: 128 Kbytes

-

RL78 family: 64 Kbytes (The available RAM is restricted to the internal RAM.)

 

There is a trial period for the first 60 days following building after the first installation of an evaluation version of a software tool.