This dialog box is used to create a new toolbar to appear in the Main window.
The following items are explained here.
In the [Toolbars] tab of the User Setting dialog box, click the [New...] button. |
Type in the name of the new toolbar directly via the keyboard.
"UltraToolbar1" is specified by default.
Select the location for the new toolbar from the following drop-down list.
The location specified here is the location where the new toolbar will appear immediately after it is created (toolbars can be moved freely by dragging and dropping).
Displays the toolbar at the top of the Main window (default). |
|
Displays the toolbar at the bottom of the Main window. |
|
Displays the toolbar on the leftedge of the Main window. |
|
Displays the toolbar on the rightedge of the Main window. |
|
Displays the toolbar above the Main window, without docking it. |
Creates a new toolbar with the specified information, and closes this dialog box. The new toolbar appears in the list on the User Setting dialog boxs [Toolbars] tab, with its check box selected. |
|