| [General - Debug] category | 
Use this category to configure general setting relating to debugging.
| 
Figure A.50 | Option Dialog Box ([General - Debug] Category) | 
 
The following items are explained here.
[How to open]
| 
- | From the [Tool] menu, select [Options...]. | 
[Description of each area]
| 
(1) | [Observe downloaded load module files changing] | 
|  | 
Monitors load module files downloaded to the debugging tool for changes.  When there is a change, a message dialog box confirming whether to execute the download is displayed. | 
|  | 
Does not monitor load module files downloaded to the debugging tool for changes (default). | 
| 
(2) | [Add source files automatically (for the "Debug Only" project only)] | 
|  | 
In a debug-dedicated project, when downloading a load module file into the debug tool, source files are automatically added to the project tree (default). | 
|  | 
In a debug-dedicated project, when downloading a load module file into the debug tool, source files are not automatically added to the project tree. | 
| 
Caution | This function is only valid when a load module file has been added to the Download files node of the project tree.When a load module file has been added in the [Download File Settings] tab on the Property panel of the debug tool, source files are not added to the project tree.
 | 
|  | 
Beeps when the execution of a user program is halted due to a break event (hardware or software break). | 
|  | 
Does not beep when the execution of a user program is halted due to a break event (hardware or software break) (default). | 
| 
(4) | [Save the value of SFRs and IORs added in the Watch 4 panel] | 
|  | 
Saves also the states of SFRs and IORs registered in the Watch 4 panel when saving the state of the debug tool.  Note that only the value of SFRs and IORs which can be read or rewritten will be saved. | 
|  | 
Does not save the states of SFRs and IORs registered in the Watch 4 panel when saving the state of the debug tool.  Note that only the value of SFRs and IORs which can be read or rewritten will be saved (default). | 
| 
Caution | This feature can be used only when there is a valid license. | 
| 
(5) | [Enable rewind feature] | 
|  | 
Automatically accumulates the memory and register values just before the debug tool is executed. | 
|  | 
Automatically accumulates the memory and register values just before the debug tool is executed (default). | 
| 
(a) | [Maximum number of times of rewinding] | 
Specify the upper limit for accumulation by the rewind feature.
Either enter a number between 1 and 100 directly via the keyboard, or specify a number via the  buttons.  The default is 50.
 buttons.  The default is 50.
Note that clicking on the [OK] or [Apply] button while this item remains blank causes the tab setting to remain at the previously saved value.
| 
Caution | This feature can be used only when there is a valid license. | 
| 
Initialize Settings | 
Returns all currently displayed setting to their default values. | 
[Function buttons]
|  |  | 
| 
Initialize All Settings | 
Restores all settings on this dialog box to their default values. 
Note, however, that newly added items in the [General - External Tools] category will not be removed. | 
| 
OK | 
Applies all setting and closes this dialog box. | 
| 
Cancel | 
Ignores the setting and closes this dialog box. | 
| 
Apply | 
Applies all setting (does not close this dialog box). | 
| 
Help | 
Displays the help of this dialog box. |