| [General - Startup and Exit] category | 
Use this category to configure general settings relating to startup and shutdown.
| 
Figure A.41 | Option Dialog Box ([General - Startup and Exit] Category) | 
 
The following items are explained here.
[How to open]
| 
- | From the [Tool] menu, select [Options...]. | 
[Description of each area]
| 
(1) | [Open the One-point Advice dialog box at CS+ startup] | 
|  | 
Shows the One Point Advice dialog box on startup (default). | 
|  | 
Does not show the One Point Advice dialog box on startup. | 
| 
(2) | [Open the Splash window at CS+ startup] | 
|  | 
Shows the Splash window on startup (default). | 
|  | 
Does not show the Splash window on startup. | 
| 
(3) | [Load the last project at CS+ startup] | 
|  | 
Automatically loads the last project on startup (default). | 
|  | 
Does not automatically load the last project on startup. | 
| 
(4) | [Reduce startup time by enabling rapid startup] | 
|  | 
Reduces startup time by enabling rapid startup (default). | 
|  | 
Disables the rapid start feature. | 
| 
Caution | This item is only enabled when this product is installed using the installer.  It is disabled when a packaged item is being used. | 
| 
Initialize Settings | 
Returns all currently displayed setting to their default values. | 
[Function buttons]
|  |  | 
| 
Initialize All Settings | 
Restores all settings on this dialog box to their default values. 
Note, however, that newly added items in the [General - External Tools] category will not be removed. | 
| 
OK | 
Applies all setting and closes this dialog box. | 
| 
Cancel | 
Ignores the setting and closes this dialog box. | 
| 
Apply | 
Applies all setting (does not close this dialog box). | 
| 
Help | 
Displays the help of this dialog box. |