2.6 Set Build Target Files

Before running a build, you must add the build target files (such as C source file or assembly source file) to the project.

This section explains operations on setting files in the project.