2.8.5  
Compile/assemble individual files
 
You can just compile or assemble for each source file added to the project.
| 
(1) | When compiling a C source file | 
Select the C source file on the project tree and select the [Compile] from the context menu.
| 
Figure 2.87 | [Compile] Item | 
 
| 
(2) | When assembling an assembly source file | 
Select the assembly source file on the project tree and select the [Assemble] from the context menu.
| 
Figure 2.88 | [Assemble] Item |