2.8.8 Delete intermediate files and generated files

You can delete all the intermediate files and generated files output by running a build (hereafter referred to as "clean").

Running a clean is performed for the entire project (main project and subprojects) or active project (see "2.7.5 Change the build target project").

(1)

When running a clean of the entire project

From the [Build] menu, select [Clean Project].

Figure 2.90

[Clean Project] Item

 

(2)

When running a clean of the active project

Select the project, and then select [Clean active project] from the context menu.

Figure 2.91

[Clean active project] Item