2.4.6  Open a project folder in Explorer
 
You can open the folder where the project file for a project (main project or subproject) is saved from the project tree in Explorer.
Select the Project node or Subproject node and select [Open Folder with Explorer] on the context menu.
Figure 2.23  | [Open Folder with Explorer] Item (For a Project)  | 
 
 
Remark  | When you select [Open Folder with Explorer] from a file's context menu, the folder the file is saved in is opened in Explorer.  |