1.3 System Configuration

Below is shown an example of the system configuration.

Figure 1.1

System Configuration

 

Remark

The emulator that can be connected differs depending on the microcontroller used in the project.
See "CS+ Integrated Development Environment Users Manual: Debug Tool" for details.