This panel is used to display components of the project (microcontroller, design tool, build tool, debug tool, etc.) in a tree structure.
The following items are explained here.
Project components are displayed in tree view with the following given node.
When the node is selected, the detailed information (property) is displayed in the Property panel, and you can change the settings. |
The following context menu items are displayed by right clicking the mouse on [Program Analyzer (Analyze Tool)] node.
|
Opens the Function List panel. |
||
|
Opens the Variable List panel. |
||
|
Opens the Analysis Chart panel. |
||
|
Opens the Call Graph panel. |
||
|
Opens the Class/Member panel. |
||
|
Opens the Property panel containing the information for the analysis tool. |
||