Reads the results of A/D conversion (8 bits; most significant 8 bits of 10-bit resolution).
[Syntax]
#include "r_cg_macrodriver.h"
void R_ADC_Get_Result_8bit ( uint8_t * const buffer );
|
[Argument(s)]
|
|
|
|
|
|
uint8_t * const buffer;
|
Pointer to area in which to store the results of A/D conversion
|
Remark | Below is an example of the results of A/D conversion to be stored in buffer. |
[Return value]
None.