3.2.28
Comparator/ProgrammableGainAmplifier
Below is a list of API functions output by the Code Generator for comparator/programmable gain amplifier use.
Table 3.28 | API Functions: [Comparator/ProgrammableGainAmplifier] |
|
|
|
|
R_COMPPGA_Create
|
Performs initialization necessary to control the comparator/programmable gain amplifier.
|
|
R_COMPPGA_Set_PowerOff
|
Halts the clock supplied to the comparator/programmable gain amplifier.
|
|
R_COMPPGA_Create_UserInit
|
Performs user-defined initialization relating to the comparator/programmable gain amplifier.
|
|
r_compn_interrupt
|
Performs processing in response to the comparator interrupt INTCMPn.
|
|
R_COMPn_Start
|
Begins comparison of reference input voltage and analog input voltage.
|
|
R_COMPn_Stop
|
Stops comparison of reference input voltage and analog input voltage.
|
|
R_PGA_Start
|
Starts the operation of programmable gain amplifier.
|
|
R_PGA_Stop
|
Ends the operation of programmable gain amplifier.
|
|
R_PWMOPT_Start
|
Supplies the clock to the 6-phase PWM option.
In addition, sets the operation mode of the 6-phase PWM option.
|
|
R_PWMOPT_Stop
|
Halts the clock supplied to the 6-phase PWM option.
|