Performs processing in response to the DALI reception error interrupt INTSREDLn.
Remark | This API function is called as the callback routine of interrupt process r_dalin_interrupt_error corresponding to the DALI reception error interrupt INTSREDLn. |
[Syntax]
#include "r_cg_macrodriver.h"
static void r_dalin_callback_error ( uint8_t err_type );
|
Remark | n is the channel number. |
[Argument(s)]
|
|
|
|
|
|
uint8_t err_type;
|
Trigger for DALI reception error interrupt
00000xx1B: Overrun error
00000x1xB: Parity error
000001xxB: Framing error
|
[Return value]
None.