|
R_RTC_Set_BinaryCounterValue
|
Sets the counter value of the real-time clock.(in the case of the binary mode setting)
[Syntax]
#include "r_cg_macrodriver.h"
#include "r_cg_rtc.h"
MD_STATUS R_RTC_Set_BinaryCounterValue ( uint32_t counter_write_val );
|
[Argument(s)]
|
|
|
|
|
|
uint32_t
counter_write_val;
|
Counter value
|
[Return value]
|
|
|
|
MD_OK
|
Normal completion
|
|
MD_BUSY1
|
Executing count process (before change to setting)
|
Remark | If MD_BUSY1 is returned, it may be because the counter operation start wait time is too short, so make the value of the RTC_WAITTIME macro defined in the header file "r_cg_rtc.h" larger. |