Performs processing in response to the CSI reception error interrupt INTSREn.
Remark | This API function is called as the callback routine of interrupt process r_uartn_interrupt_error corresponding to the CSI reception error interrupt INTSREn. |
[Syntax]
#include "r_cg_macrodriver.h"
static void r_csimn_callback_error ( uint8_t err_type );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
|
|
|
|
|
|
uint8_t err_type;
|
Trigger for CSI reception error interrupt
00000xx1B: Overrun error
|
[Return value]
None.