Obtains the second term of a bit symbol.
[Function]
Obtains the second term of a bit symbol.
[Application example]
BITSYM .EQU 0x0FE20.3
MOVW AX, #BITPOS(BITSYM) ; (1)
|
(1) | Execution of the MOVW instruction loads a value of 3 in the AX register. |
[Caution]
No bit term (see "5.1.15 Bit position specifier") can be specified in the operand field.