|
[Microcontroller Information] tab
|
This tab shows the detailed information on microcontrollers configured in the project, categorized by the following and the configuration can be changed.
(1) [File Information]
(2) [Microcontroller Information]
(3) [IOR Display Type] [RH850]
(4) [Notes]
Figure A.14 | Property Panel: [Microcontroller Information] Tab |
[Description of each category]
The detailed information on the file is shown.
|
File name
|
Displays device file name.
|
|
Default
|
Device file name
|
|
How to change
|
Changes not allowed
|
|
Absolute path
|
Displays the absolute path of the device file.
|
|
Default
|
The absolute path of the device file
|
|
How to change
|
Changes not allowed
|
(2) | [Microcontroller Information] |
The detailed information on microcontrollers is displayed and their configuration can be changed.
|
Microcontroller name
|
Displays microcontrollers to use in the project or the subproject.
|
|
Default
|
Microcontrollers used in the main project or the subproject
|
|
How to change
|
Changes not allowed
|
|
Nickname
|
Displays the nickname of the microcontroller to use.
|
|
Default
|
The nickname of the microcontroller to use
|
|
How to change
|
Changes not allowed
|
|
File version
|
Displays the device file version of the microcontroller to use.
|
|
Default
|
The device file version of the microcontroller to use
|
|
How to change
|
Changes not allowed
|
|
Bank size [KBytes]
|
Displays the bank size of the microcontroller being used in Kbytes, as a decimal number.
Note that this property is only shown for microcontrollers with a memory bank.
|
|
Default
|
The bank size recorded in your microcontroller's device file
|
|
How to change
|
Changes not allowed
|
|
Internal ROM size [KBytes]
|
Displays internal ROM size [KBytes]of the microcontroller to use in decimal number.
|
|
Default
|
Internal ROM size of the microcontroller to use
|
|
How to change
|
Changes not allowed
|
|
Internal RAM size [Bytes]
|
Displays internal RAM size [KBytes] of the microcontroller to use in decimal number.
|
|
Default
|
Internal RAM size of the microcontroller to use
|
|
How to change
|
Changes not allowed
|
|
Reset vector address
|
This is the reset vector address of the microcontroller to use.
See the user's manual of the device for the reset vector address.
Note that this property is displayed when the device has PE1 or is a single-core device.
|
|
Default
|
The peculiar value for the target device
|
|
How to change
|
Directly enter in the text box.
|
|
Restriction
|
0 to FFFFFFFF (hexadecimal number without 0x)
|
|
Reset vector address of PEn
|
This is the reset vector address of PEn of the microcontroller to use (n: core number).
See the user's manual of the device for about the reset vector address.
Note that this property is displayed when the device has PE1.
|
|
Default
|
The peculiar value for the target device
|
|
How to change
|
Directly enter in the text box.
|
|
Restriction
|
0 to FFFFFFFF (hexadecimal number without 0x)
|
(3) | [IOR Display Type] [RH850] |
The detailed information on the IOR display type is shown.
|
IOR display type
|
Displays the IOR display type of the project.
|
|
Default
|
IOR display type of the project
|
|
How to change
|
Changes not allowed
|
The detailed information on records is displayed and their configuration can be changed.
|
Memo
|
Add memos to the microcontroller information.
The memo is added one item in one line.
The added memos are displayed as subproperty.
|
|
Default
|
Memo [Number of items]
|
|
How to change
|
Edit by the Text Edit dialog box which appears when clicking the [...] button.
For the subproperty, you can use a text box directly enter the text.
|
|
Restriction
|
Up to 256 characters
Up to 256 characters are allowed.
|