To set options for the hex output phase, select the Build tool node on the project tree and select the [Hex Output Options] tab on the Property panel.
You can set the various hex output options by setting the necessary properties in this tab.
This tab is displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.00.00 or higher or when V2.00.00 or higher is selected in the [Using compiler package version] property.  | 
Often used options have been gathered under the [Frequently Used Options(for Hex Output)] category on the [Common Options] tab.  |