3.2.14
Port output enable 2 (POE2)
Below is a list of API functions output by the Code Generator for port output enable 2 use.
Table 3.14 | API Functions: [Port Output Enable 2] |
|
|
|
|
R_POE2_Create
|
Performs initialization necessary to control the port output enable 2.
|
|
R_POE2_Create_UserInit
|
Performs user-defined initialization relating to the port output enable 2.
|
|
r_poe2_oein_interrupt
|
Performs processing in response to the output enable interrupt n (OEIn).
|
|
R_POE2_Start
|
Places the MTU's complementary PWM output pins in the high-impedance state.
|
|
R_POE2_Stop
|
Releases the R_POE2_Stop MTU's complementary PWM output pins from the high-impedance state.
|
|
R_POE2_Set_HiZ_MTUn
|
Sets the high-impedance state for the MTUn pins.
|
|
R_POE2_Clear_HiZ_MTUn
|
Clear the high-impedance state for the MTUn pins
|