| 
 Compiler Options That Become Invalid 
 | 
In addition to the options in 2.5.4  Library Generator Options, the C/C++ compiler options can be specified in the library generator as options used for library compilation. However, the options listed below are invalid; they are not selected at library compilation.
Table 2.19  | Invalid Options  | 
 
| 
 | 
 | 
 | 
 | 
| 
 
1 
 | 
 
lang 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
2 
 | 
 
include 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
3 
 | 
 
define 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
4 
 | 
 
undefined 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
5 
 | 
 
message 
nomessage 
 | 
 
Always invalid 
 | 
 
nomessage 
 | 
| 
 
6 
 | 
 
change_message 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
7 
 | 
 
file_inline_path 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
8 
 | 
 
comment 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
9 
 | 
 
check 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
10 
 | 
 
output 
 | 
 
Always invalid 
 | 
 
output=obj 
 | 
| 
 
11 
 | 
 
noline 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
12 
 | 
 
debug 
nodebug 
 | 
 
Always invalid 
 | 
 
nodebug 
 | 
| 
 
13 
 | 
 
listfile 
nolistfile 
show 
 | 
 
Always invalid 
 | 
 
nolistfile 
 | 
| 
 
14 
 | 
 
file_inline 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
15 
 | 
 
asmcmd 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
16 
 | 
 
lnkcmd 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
17 
 | 
 
asmopt 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
18 
 | 
 
lnkopt 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
19 
 | 
 
logo 
nologo 
 | 
 
Always invalid 
 | 
 
nologo 
 | 
| 
 
20 
 | 
 
euc 
sjis 
latin1 
utf8 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
21 
 | 
 
outcode 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
22 
 | 
 
subcommand 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
23 
 | 
 
alias 
 | 
 
Always invalid 
 | 
 
alias=noansi 
 | 
| 
 
24 
 | 
 
pic 
pid 
 | 
 
lang=cpp or at C++ source compilationNote1 
 | 
 
None 
 | 
| 
 
25 
 | 
 
ip_optimize 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
26 
 | 
 
merge_files 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
27 
 | 
 
whole_program 
 | 
 
Always invalid 
 | 
 
None 
 | 
| 
 
28 
 | 
 
big5 
gb2312 
 | 
 
Always invalid Note2 
 | 
 
None 
 | 
 
Notes 1.  | Warning W0511171 is output.  | 
 
Notes 2.  | Error F0593305 is output. (This library cannot be generated.)  |