|
BNOT
|
Inverting a bit
|
BNOT
|
|
Bit NOT
|
[Syntax]
BNOT src, dest
[Operation]
(1)When dest is a memory location:
unsigned char dest;
dest ^= ( 1 << ( src & 7 ));
(2)When dest is a register:
register unsigned long dest;
dest ^= ( 1 << ( src & 31 ));
[Function]
- | This instruction inverts the value of the bit of dest, which is specified by src, and places the result into the specified bit. |
- | The immediate value given as src is the number (position) of the bit.
The range for IMM:3 operands is 0 ≤ IMM:3 ≤ 7. The range for IMM:5 is 0 ≤ IMM:5 ≤ 31. |
[Instruction Format]
|
|
|
|
|
|
|
(1)BNOT src, dest
|
|
#IMM:3
|
[Rd].B
|
|
|
|
#IMM:3
|
dsp:8[Rd].B
|
|
|
|
#IMM:3
|
dsp:16[Rd].B
|
|
|
|
Rs
|
[Rd].B
|
|
|
|
Rs
|
dsp:8[Rd].B
|
|
|
|
Rs
|
dsp:16[Rd].B
|
|
|
(2)BNOT src, dest
|
|
#IMM:5
|
Rd
|
|
|
|
Rs
|
Rd
|
|
|
|
Rs
|
dsp:16[Rd].B
|
|
[Flag Change]
This instruction does not affect the states of flags.
[Description Example]
BNOT #7, [R2]
BNOT R1, [R2]
BNOT #31, R2
BNOT R1, R2