(1)  | When the file name and line number are included  | 
 
file-name (line-number) : message-type component-number message-number : message 
 | 
 
(2)  | When the file name and line number aren't included  | 
 
message-type component-number message-number : message 
 | 
 
Remark  | Following contents are output as the continued character string.  | 
 
MESSAGE TYPES														:	1 alphabetic character
COMPONENT NUMBERS														:	05
MESSAGE NUMBERS														:	5 digits