By using expanded function object with high efficiency can be created.
Here, two methods are described for shifting to the CCRX from other C compiler and shifting to C compiler from the CCRX.
<From other C compiler to the CCRX>
C source needs to be modified, when C compiler supports the #pragma. Modification methods are examined according to the C compiler specifications.
It should be modified when other C compilers are expanding the specifications such as adding keywords etc. Modified methods are examined according to the C compiler specifications.
#pragma is one of the pre-processing directives supported by ANSI. The character string next to #pragma is made to be recognized as directives to C compiler. If that directive does not supported by the compiler, #pragma directive is ignored and the compiler continues the process and ends normally.  | 
<From the CCRX to other C compiler>
The CCRX, either deletes key word or divides # fdef in order shift to other C compiler as key word has been added as expanded function.  |