M0520009 |
[Message] |
Nested comment is not allowed. |
M0520018 |
[Message] |
Expected a ")". |
M0520111 |
[Message] |
Statement is unreachable. |
M0520128 |
[Message] |
Loop is not reachable from preceding code. |
M0520174 |
[Message] |
Expression has no effect. |
M0520193 |
[Message] |
Zero used for undefined preprocessing identifier xxx. |
M0520237 |
[Message] |
Selector expression is constant. |
M0520261 |
[Message] |
Access control not specified ("name" by default). |
M0520324 |
[Message] |
Duplicate friend declaration. |
M0520381 |
[Message] |
Extra ";" ignored. |
M0520399 |
[Message] |
name has an operator new xxx() but no default operator delete xxx(). |
M0520400 |
[Message] |
name has a default operator delete xxx() but no operator new xxx(). |
M0520479 |
[Message] |
name redeclared "inline" after being called. |
M0520487 |
[Message] |
Inline name cannot be explicitly instantiated. |
M0520534 |
[Message] |
Use of a local type to specify an exception. |
M0520535 |
[Message] |
Redundant type in exception specification. |
M0520549 |
[Message] |
symbol is used before its value is set. |
M0520618 |
[Message] |
Struct or union declares no named members. |
M0520652 |
[Message] |
Calling convention is ignored for this type. |
M0520678 |
[Message] |
Call of "symbol" cannot be inlined. |
M0520679 |
[Message] |
symbol cannot be inlined. |
M0520815 |
[Message] |
Type qualifier on return type is meaningless. |
M0520831 |
[Message] |
Support for placement delete is disabled. |
M0520863 |
[Message] |
Effect of this "#pragma pack" directive is local to xxx. |
M0520866 |
[Message] |
Exception specification ignored. |
M0520949 |
[Message] |
Specifying a default argument on this declaration is nonstandard. |
M0521348 |
[Message] |
Declaration hides "symbol". |
M0521353 |
[Message] |
symbol has no corresponding member operator delete xxx (to be called if an exception is thrown during initialization of an allocated object). |
M0521380 |
[Message] |
Virtual xxx was not defined (and cannot be defined elsewhere because it is a member of an unnamed namespace). |
M0521381 |
[Message] |
Carriage return character in source line outside of comment or character/string literal. |
M0523009 |
[Message] |
This pragma has no effect. |
M0523028 |
[Message] |
Rule rule number : description |
[Explanation] |
Violation of a MISRA-C:2004 rule (indicated by the rule number and description) was detected. |
M0523033 |
[Message] |
Precision lost. |
M0523086 |
[Message] |
Rule rule number : description |
[Explanation] |
Violation of a MISRA-C:2012 rule (indicated by the rule number and description) was detected. |
M0560001 |
[Message] |
Section "section" created by optimization "optimization" |
[Explanation] |
The section named section was created as a result of the optimization. |
M0560002 |
[Message] |
Symbol "symbol" created by optimization "optimization" |
[Explanation] |
The symbol named symbol was created as a result of the optimization. |
M0560004 |
[Message] |
"file"-"symbol" deleted by optimization |
[Explanation] |
As a result of symbol_delete optimization, the symbol named symbol in file was deleted. |
M0560005 |
[Message] |
The offset value from the symbol location has been changed by optimization : "file"-"section"-"symbol + offset" |
[Explanation] |
As a result of the size being changed by optimization within the range of symbol + offset, the offset value was changed. Check that this does not cause a problem. To disable changing of the offset value, cancel the specification of the goptimize option on assembly of file. |
M0560100 |
[Message] |
No inter-module optimization information in "file" |
[Explanation] |
No inter-module optimization information was found in file. Inter-module optimization is not performed on file. To perform inter-module optimization, specify the goptimize option on compiling and assembly. |
M0560101 |
[Message] |
No stack information in "file" |
[Explanation] |
No stack information was found in file. file may be an assembler output file. The contents of the file will not be in the stack information file output by the linker. |
M0560102 |
[Message] |
Stack size "size" specified to the undefined symbol "symbol" in "file" |
[Explanation] |
Stack size size is specified for the undefined symbol named symbol in file. |
M0560103 |
[Message] |
Multiple stack sizes specified to the symbol "symbol" |
[Explanation] |
Multiple stack sizes are specified for the symbol named symbol. |
M0560300 |
[Message] |
Mode type "mode type1" in "file" differ from "mde type2" |
[Explanation] |
A file with a different mode type was input. |
M0560400 |
[Message] |
Unused symbol "file"-"symbol" |
[Explanation] |
The symbol named symbol in file is not used. |
M0560500 |
[Message] |
Generated CRC code at "address" |
[Explanation] |
CRC code was generated at address. |
M0560510 |
[Message] |
Section "section" was moved other area specified in option "cpu=<attribute>" |
[Explanation] |
section without dividing is allocated according to cpu=<attribute>. |
M0560511 |
[Message] |
Sections "section name","new section name" are Non-contiguous |
[Explanation] |
section was divided and the newly created section is new section name. |
M0560512 |
[Message] |
Section "section" created by "option" |