Renesas Electronics
top
FUNCTIONS
Other Notes on Usage [E1] [E20] [EZ Emulator]
2.22
Other Notes on Usage [E1] [E20] [EZ Emulator]
Previous Topic
Differences between the Microcontroller and the Emulator
Next Topic
Internal Flash ROM
Table of Contents
Overview
Preparation before Debugging
Configuration of Operating Environment of the Debug Tool
Connect to/Disconnect from the Debug Tool
Download and Upload
Displaying and Changing Programs
Usage of PIC/PID Function
Setting Overlay Sections
Execute Programs
Stop Programs (Break)
Displaying and Changing Memory, Registers, and Variables
Display Function Call Information from the Stack
Collecting an Execution History
Measuring the Execution Time
Measure Coverage [Simulator] [E20 [RX71M and RX64M Groups]]
Set an Action into Programs
Event Management
Setting Up the Hook Process
Using the Debug Console
About Input Value
Differences between the Microcontroller and the Emulator
Other Notes on Usage [E1] [E20] [EZ Emulator]
Internal Flash ROM
FINE interface
Endian select registers (MDEB, MDES) [RX71M, RX651, RX65N, RX64M, RX62x, RX630, RX631, RX63N, RX63T, RX634, RX210, RX21A, RX220, RX23x, RX24T, RX110, RX111, RX113, RX130]
Option function select register 1 (OFS1) setting [RX62x, RX630, RX631, RX63N, RX63T, RX634, RX210, RX21A, RX220, RX23x, RX24T, RX130]
Option function select register 1 (OFS1) setting [RX110, RX111, RX113]
Option function select register 1 (OFS1) setting [RX71M, RX651, RX65N, RX64M]
Register values after the flash memory has been programmed
DMAC and DTC
High-speed clock oscillator (HOCO) [RX71M, RX64M, RX210, RX21A, RX220]
Lock bits [For microcontrollers with lock bits]
Area protection [For microcontrollers that support the area protection]
Operating frequency
Start up program protection function [RX23T, RX24T, RX110, RX111, RX113, RX130]
Access to the MPU area [For microcontrollers with memory-protection unit (MPU)]
Reset microcontroller (CPU)
Memory access in on-chip ROM disabled extended mode
Event combination condition [RX71M, RX64M, RX651, RX65N]
Coverage measurement function [E20 [RX71M, RX64M, RX651, RX65N]]
Trace function
Trusted Memory [RX71M, RX64M, RX651, RX65N]
FSPR bit in the FAW register [RX651, RX65N]
ROM cache function [RX651, RX65N, RX24T]