Renesas Electronics
top
FUNCTIONS
Manipulate a Project
2.4
Manipulate a Project
This section describes how to manipulate a project.
Previous Topic
Create a project for multi-core [RH850]
Next Topic
Open a project
Table of Contents
Overview
Start CS+
Create a Project
Manipulate a Project
Open a project
Add an existing subproject
Project is added to the favorites menu
Remove a subproject from the project
Change the project name
Open a project folder in Explorer
Set the build order of projects
Open a CubeSuite+ project
Convert a CA78K0R project into a CC-RL project
Convert an e2 studio project into a CS+ project [RX][RL78]
Convert a CubeSuite project into a CS+ project
Convert a HEW project into a CS+ project
Convert a PM+ project into a CS+ project
Change the microcontroller
Change the Build Tool Version
Set Build Target Files
Make Settings for Build Operations
Run a Build
Save the Project File
Change the Window Layout
Accelerate the Startup Time of CS+
Manipulate CS+ on the Command Line