M0523028 |
[Message] |
Rule rule number : description |
[Explanation] |
Violation of a MISRA-C:2004 rule (indicated by the rule number and description) was detected. |
M0523086 |
[Message] |
Rule rule number : description |
[Explanation] |
Violation of a MISRA-C:2012 rule (indicated by the rule number and description) was detected. |
M0560101 |
[Message] |
No stack information in "file" |
[Explanation] |
No stack information was found in file. file may be an assembler output file. The contents of the file will not be in the stack information file output by the optimizing linker. |
M0560102 |
[Message] |
Stack size "size" specified to the undefined symbol "symbol" in "file" |
[Explanation] |
Stack size size is specified for the undefined symbol named symbol in file. |
M0560103 |
[Message] |
Multiple stack sizes specified to the symbol "symbol" |
[Explanation] |
Multiple stack sizes are specified for the symbol named symbol. |
M0560300 |
[Message] |
Mode type "mode type1" in "file" differ from "mde type2" |
[Explanation] |
A file with a different mode type was input. |
M0560400 |
[Message] |
Unused symbol "file"-"symbol" |
[Explanation] |
The symbol named symbol in file is not used. |
M0560500 |
[Message] |
Generated CRC code at "address" |
[Explanation] |
CRC code was generated at address. |
M0560510 |
[Message] |
Section "section" was moved other area specified in option "cpu=<attribute>" |
[Explanation] |
section without dividing is allocated according to cpu=<attribute>. |
M0560511 |
[Message] |
Sections "section name","new section name" are Non-contiguous |
[Explanation] |
section was divided and the newly created section is new section name. |
M0560512 |
[Message] |
Section "section" created by "option" |
M0560700 |
[Message] |
Section address overflow out of range : "section" |
[Explanation] |
The address of "section" is beyond the allowable address range. |