Column Chooser dialog box

This dialog box sets the type of the items to be displayed as the CPU usage status in the Analysis information table area on the Analysis Result panel.

Figure A-7. Column Chooser Dialog Box



The following items are explained here.

- [How to open]

- [Description of each area]

- [Function buttons]

[How to open]

- Press the button located in the upper left corner of the Analysis information table area on the Analysis Result panel.

[Description of each area]

(1) Item select area

Selects whether or not to display the applicable items in the Analysis information table area on the Analysis Result panel.

Checked

Displays the applicable items in the Analysis information table area on the Analysis Result panel.

Not checked

Hides the applicable items from the Analysis information table area on the Analysis Result panel.



[Function buttons]

Button

Function

Default

Resets the item types and their sorting order displayed in the Analysis information table area on the Analysis Result panel to their default condition.

Close

Closes this dialog box.