This is the first window to open when CS+ is launched.
In this window. you can open panels for the analysis tool.
The following items are explained here.
In Windows 8 or Windows 8.1, select [CS+ for CC (RL78,RX,RH850)] on the start screen.  | 
The [View] menu for the analysis tool provides the following items and functions (default).
| 
 Opens the Output panel.  | 
||
| 
 The following cascade menus are displayed to open panels for the analysis tool.  | 
||
| 
 Opens the Function List panel.  | 
||
| 
 Opens the Variable List panel.  | 
||
| 
 Opens the Analysis Chart panel.  | 
||
| 
 Opens the Call Graph panel.  | 
||
| 
 Opens the Class/Member panel.  | 
||
The toolbar for the analysis tool provides the following items and functions (default).
| 
 Opens the Function List panel. The function of this item is the same as that of [Function List] in the [View] menu.  | 
|
| 
 Opens the Variable List panel. The function of this item is the same as that of [Variable List] in the [View] menu.  | 
|
| 
 Opens the Analysis Chart panel. The function of this item is the same as that of [Analysis Chart] in the [View] menu.  | 
|
| 
 Opens the Call Graph panel. The function of this item is the same as that of [Call Graph] in the [View] menu.  | 
|
| 
 Opens the Class/Member panel. The function of this item is the same as that of [Class/Member] in the [View] menu.  | 
This area consists of multiple panels, each dedicated to a different purpose.
See the following sections for details on a panel used by the analysis tool.