2.7 Set Hex Output Options

To set options for the hex output phase, select the Build tool node on the project tree and select the [Hex Output Options] tab on the Property panel.

You can set the various hex output options by setting the necessary properties in this tab.

Caution 1.

This tab is not displayed for the library project.

Caution 2.

This tab is displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.00.00 or higher or when V2.00.00 or higher is selected in the [Using compiler package version] property.
When the version of the compiler package is V2.00.00 or lower, the properties from this tab are included in the [Convert Load Module File] category from the [Link Options] tab. See "Property panel" in "A. WINDOW REFERENCE" for details.

Figure 2.56

Property Panel: [Hex Output Options] Tab

 

Remark

Often used options have been gathered under the [Frequently Used Options(for Hex Output)] category on the [Common Options] tab.