r_atuiv_timerknm_icrnx_interrupt


Performs processing in response to the ICRnx register interrupt.

[Syntax]

void    r_atuiv_timerknm_icrnx_interrupt ( void );

Remark

k is the timer kind, n is the unit number, m is the channel number, x is the register number.

[Argument(s)]

None.

[Return value]

None.