Renesas Electronics
R_CGC_Create_UserInit
Performs user-define initialization relating to the clock generator (include reset function, on-chip debug function, etc.).
Remark
This API function is called as the R_CGC_Create callback routine.
[Syntax]
void R_CGC_Create_UserInit ( void );
[Argument(s)]
None.
[Return value]