Renesas Electronics
r_sci3m_callback_error
Performs processing in response to the SCI error interrupt.
Remark
This API function is called as the callback routine of interrupt process r_sci3m_interrupt_error corresponding to the SCI error interrupt.
[Syntax]
void r_SCI3m_callback_error ( void );
m is the channel number.
[Argument(s)]
None.
[Return value]