R_TAUDn_Create_UserInit


Performs user-defined initialization relating to the timer array unit Dn.

Remark

This API functions is called as the R_TAUDn_Create callback routine.

[Syntax]

void    R_TAUDn_Create_UserInit ( void );

Remark n is the unit number.

[Argument(s)]

None.

[Return value]

None.