R_ADC_Set_TestChannel


Sets the operation mode of A/D converter.

[Syntax]

#include    "r_cg_macrodriver.h"
#include    "r_cg_adc.h"
MD_STATUS   R_ADC_Set_TestChannel ( test_channel_t channel );

[Argument(s)]

I/O

Argument

Description

I

test_channel_t  channel;

Operation mode of A/D converter

ADNORMALINPUT: Normal mode (Normal A/D conversion)

ADAVREFM: Test mode (AVREFM input)

ADAVREFP: Test mode (AVREFP input)

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument specification