Halts the clock supplied to the comparator/programmable gain amplifier.
Remark | Calling this API function changes the comparator/programmable gain amplifier to reset status.
For this reason, writes to the control registers after this API function is called are ignored.
|
[Syntax]
void R_COMPPGA_Set_PowerOff ( void );
|
[Argument(s)]
None.
[Return value]
None.