r_hofc_interrupt


Performs processing in response to the timer interrupt.

Remark

This API function is called as the interrupt process corresponding to the High-speed on-chip Oscillator clock Frequency Correction function interrupt INTCR.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_hofc_interrupt ( void );

 

CC-RL Compiler

static  void  __near r_hofc_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.