R_IT_Create_UserInit


Performs user-defined initialization relating to the 12-bit interval timer.

Remark

This API function is called as the R_IT_Create callback routine.

[Syntax]

void    R_IT_Create_UserInit ( void );

[Argument(s)]

None.

[Return value]

None.