Halts the clock supplied to the LCD controller/driver.
Remarks 1. | Calling this API function changes the LCD controller/driver to reset status.
For this reason, writes to the control registers after this API function is called are ignored.
|
Remarks 2. | This API function stops the clock supply to the LCD controller/driver, by operating the RTCEN bit of peripheral enable register n.
For this reason, this API function also stops the clock supply to other peripheral devices sharing the RTCEN bit (e.g. real-time clock).
|
[Syntax]
void R_LCD_Set_PowerOff ( void );
|
[Argument(s)]
None.
[Return value]
None.