R_MAC32Bit_MACUnsigned


Operates the unsigned multiply-accumulate.

[Syntax]

#include     “r_cg_macrodriver.h”
#include    “r_cg_mac32bit.h”
void    R_MAC32Bit_MACUnsigned(uint32_t data_a, uint32_t data_b, mac32bit_uint64_t * buffer_64bit);

[Argument(s)]

I/O

Argument

Description

I

uint32_t data_a

Multiplicand

I

uint32_t data_b

Multiplier

O

mac32bit_uint64_t
 * buffer_64bit

Accumulation initial value/Multiplier result

Remark

See R_MAC32bit_MULUnsigned for details about the mac32bit_uint64_t.

[Return value]

None.