r_pga_dsad_interrupt_scan
|
Performs processing in response to the 24-bit ΔΣ A/D scan end interrupt INTDSADS.
Remark | This API function is called as the interrupt process corresponding to the 24-bit ΔΣ A/D scan end interrupt INTDSADS. |
[Syntax]
CA78K0R Compiler