|
R_TMRDn_ForcedOutput_Stop
|
Ends the pulse output forced cutoff for 16-bit timer RDn.
Remark | This API function can only be called when the 16-bit timer RDn is the count to stopped (the TSTART bit in the timer RD start register (TRDSTR) is 0). |
[Syntax]
void R_TMRDn_ForcedOutput_Stop ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.