R_DOC_GetResult


Gets the result of operation.

[Syntax]

#include    "r_cg_macrodriver"
void    R_DOC_GetResult ( uint16_t * const data );

[Argument(s)]

I/O

Argument

Description

O

uint16_t  * const data;

Pointer to the location where the result of operation is to be stored

[Return value]

None.