r_icu_irqn_interrupt


Performs processing in response to the external pin interrupts.

Remark

This API function is called to run interrupt processing for the external pin interrupts.

[Syntax]

static  void    r_icu_irqn_interrupt ( void );

Remark

n is the source number.

[Argument(s)]

None.

[Return value]

None.