R_LPC_ChangeSleepModeRetrunClock
|
Sets the clock source that is selected following release from sleep mode.
[Syntax]
#include "r_cg_macrodriver.h"
#include "r_cg_lpc.h"
MD_STATUS R_LPC_ChangeSleepModeReturnClock ( return_clock_t clock );
|
[Argument(s)]
|
|
|
|
return_clock_t clock;
|
Clock source type
RETURN_LOCO: Low-speed on-chip oscillator
RETURN_HOCO: High-speed on-chip oscillator
RETURN_MAIN_CLOCK: Main clock oscillator
RETURN_DISABLE: Switching of the clock source does not proceed.
|
[Return value]
|
|
MD_OK
|
Normal completion
|
MD_ERROR1
|
Change to the low-speed operating mode ended abnormally.
|
MD_ARGERROR
|
Invalid argument clock specification
|