Channel number
ADCHANNEL0: Input channel AN000
ADCHANNEL1: Input channel AN001
ADCHANNEL2: Input channel AN002
ADCHANNEL3: Input channel AN003
ADCHANNEL4: Input channel AN004
ADCHANNEL6: Input channel AN006
ADCHANNEL8: Input channel AN008
ADCHANNEL9: Input channel AN009
ADCHANNEL10: Input channel AN010
ADCHANNEL11: Input channel AN011
ADCHANNEL12: Input channel AN012
ADCHANNEL13: Input channel AN013
ADCHANNEL14: Input channel AN014
ADCHANNEL15: Input channel AN015
ADTEMPSENSOR: Extended analog input (temperature sensor output)
ADINTERREFVOLT: Extended analog input (internal reference voltage)
|