Performs processing in response to the undefined instruction exception.
Remark | This API function is called to run interrupt processing in response to an undefined instruction exception occurred when detecting the undefined instruction (unimplemented instruction) execution. |
[Syntax]
void r_undefined_exception ( void );
|
[Argument(s)]
None.
[Return value]
None.