rcv_mbx

Outline

Receive from mailbox (waiting forever).

C format

 ER      rcv_mbx (ID mbxid, T_MSG **ppk_msg);
Parameter(s)

I/O

Parameter

Description

I

 ID      mbxid;
ID number of the mailbox.

O

 T_MSG   **ppk_msg;
Start address of the message packet received from the mailbox.



[Message packet T_MSG for TA_MFIFO attribute ]

 typedef struct {
     VP      msghead;       /*RI600V4 management area*/
 } T_MSG;


[Message packet T_MSG_PRI for TA_MPRI attribute]

 typedef struct {
     T_MSG   msgque;        /*Message header*/
     PRI     msgpri;        /*Message priority*/
 } T_MSG_PRI;


Explanation

This service call receives a message from the mailbox specified by parameter mbxid, and stores its start address in the area specified by parameter ppk_msg.

If no message could be received from the target mailbox (no messages were queued to the wait queue) when this service call is issued, this service call does not receive messages but queues the invoking task to the target mailbox wait queue and moves it from the RUNNING state to the WAITING state (message reception wait state).

The receiving WAITING state for a mailbox is cancelled in the following cases.

Receiving WAITING State for a Mailbox Cancel Operation

Return Value

A message was transmitted to the target mailbox as a result of issuing snd_mbx.

E_OK

A message was transmitted to the target mailbox as a result of issuing isnd_mbx.

E_OK

Forced release from waiting (accept rel_wai while waiting).

E_RLWAI

Forced release from waiting (accept irel_wai while waiting).

E_RLWAI



Note Invoking tasks are queued to the target mailbox wait queue in the order defined during configuration (FIFO order or current priority order).

Return value

Macro

Value

Description

E_OK

0

Normal completion.

E_ID

-18

Invalid ID number.

- mbxid < 0

- mbxid > VTMAX_MBX

E_CTX

-25

Context error.

- This service call was issued from a non-task.

- This service call was issued in the CPU locked state.

- This service call was issued in the dispatching disabled state.

- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".

E_RLWAI

-49

Forced release from the WAITING state.

- Accept rel_wai/irel_wai while waiting.