ref_mpf

iref_mpf

Outline

Reference fixed-sized memory pool state.

C format

 ER      ref_mpf (ID mpfid, T_RMPF *pk_rmpf);
 ER      iref_mpf (ID mpfid, T_RMPF *pk_rmpf);
Parameter(s)

I/O

Parameter

Description

I

 ID      mpfid;
ID number of the fixed-sized memory pool.

O

 T_RMPF  *pk_rmpf;
Pointer to the packet returning the fixed-sized memory pool state.



[Fixed-sized memory pool state packet: T_RMPF]

 typedef struct  t_rmpf {
     ID      wtskid;         /*Existence of waiting task*/
     UINT    fblkcnt;        /*Number of free memory blocks*/
 } T_RMPF;


Explanation

Stores fixed-sized memory pool state packet (ID number of the task at the head of the wait queue, number of free memory blocks, etc.) of the fixed-sized memory pool specified by parameter mpfid in the area specified by parameter pk_rmpf.

- wtskid
Stores whether a task is queued to the fixed-size memory pool.

TSK_NONE: No applicable task

Value: ID number of the task at the head of the wait queue

- fblkcnt
Stores the number of free memory blocks.

Return value

Macro

Value

Description

E_OK

0

Normal completion.

E_ID

-18

Invalid ID number.

- mpfid < 0

- mpfid > VTMAX_MPF

E_CTX

-25

Context error.

- This service call was issued in the CPU locked state.

- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".

Note When the iref_mpf is issued from task or the ref_mpf is issued from non-task, the context error is not detected and normal operation of the system is not guaranteed.