-
ter_tsk
-
ER ter_tsk (ID tskid);
This service call forcibly moves the task specified by parameter
tskid to the DORMANT state.
As a result, the target task is excluded from the RI600V4 scheduling subject.
At this time, processing described in
Table 18-3 is done.
If an activation request has been queued to the target task (the activation request counter > 0) when this service call is issued, this service call moves the task to the DORMANT state, decrements the activation request counter (by subtracting 1 from the activation request counter), and then moves the task from the DORMANT state to the READY state. At this time, processing described in
Table 18-2 is done.
Note This service call does not have the function to automatically free the resources except the mutex hitherto occupied by the task (e.g., semaphores and memory blocks). Make sure the task frees these resources before it terminates
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
- This service call was issued in the CPU locked state.
- This service call was issued from non-task.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
|
|
|
|
Illegal service call use.
- Specified task is the invoking task.
|
|
|
|
- Specified task is in the DORMANT state.
|